ResizePlaneBuilder Class¶
-
class
NXOpen.Features.
ResizePlaneBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ResizePlane
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateResizePlaneBuilder()
New in version NX6.0.3.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns the plane |
ResizeDuringUpdate | Returns or sets the flag for resizing a datum plane. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCornerPoints | Gets the four corner points for resizing a datum plane |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetCornerPoints | Sets the four corner points for resizing a datum plane |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Plane¶
-
ResizePlaneBuilder.
Plane
¶ Returns the plane
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.SelectDatumPlane
New in version NX6.0.3.
License requirements: None.
ResizeDuringUpdate¶
-
ResizePlaneBuilder.
ResizeDuringUpdate
¶ Returns or sets the flag for resizing a datum plane.
If true, the datum plane is set to a default size
-------------------------------------
Getter Method
Signature
ResizeDuringUpdate()
Returns: Return type: bool New in version NX6.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResizeDuringUpdate(resizeDuringUpdate)
Parameters: resizeDuringUpdate (bool) – New in version NX6.0.3.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
GetCornerPoints¶
-
ResizePlaneBuilder.
GetCornerPoints
¶ Gets the four corner points for resizing a datum plane
Signature
GetCornerPoints()
Returns: x,y,z coordinates of corner points Return type: list of NXOpen.Point3d
New in version NX6.0.3.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetCornerPoints¶
-
ResizePlaneBuilder.
SetCornerPoints
¶ Sets the four corner points for resizing a datum plane
Signature
SetCornerPoints(cornerPoints)
Parameters: cornerPoints (list of NXOpen.Point3d
) – x,y,z coordinates of corner pointsNew in version NX6.0.3.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
ResizePlaneBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.