ReplaceFeatureBuilderMappingMethodType Enumeration

NXOpen.Features.ReplaceFeatureBuilder.MappingMethodType is an alias for NXOpen.Features.ReplaceFeatureBuilderMappingMethodType

class NXOpen.Features.ReplaceFeatureBuilderMappingMethodType

Bases: object

Type of mapping method to be used for replace feature

Enum Members

Enum Member Enum Member Description
MapOnlyObjectsWithModelingDependencies
MapAllObjects
Not supported yet
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.