ReplaceFaceBuilderReplaceTypes Enumeration

NXOpen.Features.ReplaceFaceBuilder.ReplaceTypes is an alias for NXOpen.Features.ReplaceFaceBuilderReplaceTypes

class NXOpen.Features.ReplaceFaceBuilderReplaceTypes

Bases: object

Enumeration of replace face type, don’t use it until nx502

New in version NX5.0.2.

Enum Members

Enum Member Enum Member Description
Replace
This stands for replace type - to replace the surface of the target face with the tool face
Simplify
This stands for simplify type - to simplify the geometry representation of a surface of a face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.