RefitFaceBuilderTypes Enumeration

NXOpen.Features.RefitFaceBuilder.Types is an alias for NXOpen.Features.RefitFaceBuilderTypes

class NXOpen.Features.RefitFaceBuilderTypes

Bases: object

the type of face refit

Enum Members

Enum Member Enum Member Description
Refit
refit face
FitToTarget
refit face to target
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.