RasterImageMaxTextureSize Enumeration¶
NXOpen.Features.RasterImage.MaxTextureSize is an alias for NXOpen.Features.RasterImageMaxTextureSize
-
class
NXOpen.Features.
RasterImageMaxTextureSize
¶ Bases:
object
Specifies the maximum number of pixels to allow for the width or height of a raster image.
If a size is requested which is larger than what the hardware can supported, the largest supported size will be used. All hardware can support at least 512x512 pixels.
Enum Members
Enum Member Enum Member Description N512 512 x 512 max sizeN1024 1024 x 1024 max sizeN2048 2048 x 2048 max sizeN4096 4096 x 4096 max sizeN8192 8192 x 8192 max sizeN16384 16384 x 16384 max sizeN32768 32768 x 32768 max size-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-