RapidSurfaceBuilderLoopTypes Enumeration

NXOpen.Features.RapidSurfaceBuilder.LoopTypes is an alias for NXOpen.Features.RapidSurfaceBuilderLoopTypes

class NXOpen.Features.RapidSurfaceBuilderLoopTypes

Bases: object

the subdivision loop types

Enum Members

Enum Member Enum Member Description
FourSided
subdivide four sided loops
ThreeSided
subdivide three sided loops
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.