RPOBuilderAssociativityType Enumeration

NXOpen.Features.RPOBuilder.AssociativityType is an alias for NXOpen.Features.RPOBuilderAssociativityType

class NXOpen.Features.RPOBuilderAssociativityType

Bases: object

Represents the associativity type for a dimension entity

Enum Members

Enum Member Enum Member Description
EndPoint
End-point (determined from 3d help point)
ArcCenter
Arc-center
Tangency
Tangency
EndPoint1
1st end point (at minimum parameter value)
EndPoint2
2nd end point
VerticalCenterline1
vertical centerline end point 1
VerticalCenterline2
vertical centerline end point 2
HorizontalCenterline1
horizontal centerline end point 1
HorizontalCenterline2
horizontal centerline end point 2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.