ProjectCurveBuilderArcLengthType Enumeration

NXOpen.Features.ProjectCurveBuilder.ArcLengthType is an alias for NXOpen.Features.ProjectCurveBuilderArcLengthType

class NXOpen.Features.ProjectCurveBuilderArcLengthType

Bases: object

Represents Equal Arc Length type

Enum Members

Enum Member Enum Member Description
BothXY
Represents Both X and Y
FirstXThenY
Represents First X then Y
FirstYThenX
Represents First Y then X
XOnly
Represents X only
YOnly
Represents Y only
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.