PolylineBuilderWCSOptionType Enumeration

NXOpen.Features.PolylineBuilder.WCSOptionType is an alias for NXOpen.Features.PolylineBuilderWCSOptionType

class NXOpen.Features.PolylineBuilderWCSOptionType

Bases: object

WCS principal axis or plane types

Enum Members

Enum Member Enum Member Description
X
Along X axis
Y
Along Y axis
Z
Along Z axis
YZ
In YZ plane
XZ
In XZ plane
XY
In XY plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.