PolylineBuilderMovementMethodType Enumeration

NXOpen.Features.PolylineBuilder.MovementMethodType is an alias for NXOpen.Features.PolylineBuilderMovementMethodType

class NXOpen.Features.PolylineBuilderMovementMethodType

Bases: object

Points movement types

Enum Members

Enum Member Enum Member Description
WCS
Movement along WCS principal axis or plane
View
Movement in view plane
Vector
Movement along arbitrary direction
Plane
Movement in arbitrary plane
Segment
Movement along a segment of the polyline
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.