PointSetBuilderTypes Enumeration¶
NXOpen.Features.PointSetBuilder.Types is an alias for NXOpen.Features.PointSetBuilderTypes
-
class
NXOpen.Features.
PointSetBuilderTypes
¶ Bases:
object
The settings for the type of Point Set feature.
Enum Members
Enum Member Enum Member Description CurvePoints Create points along curve.SplinePoints Create points along spline.FacePoints Create points on faceIntersectionPoints Create intersection points-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-