PointSetBuilderSplinePointsType Enumeration

NXOpen.Features.PointSetBuilder.SplinePointsType is an alias for NXOpen.Features.PointSetBuilderSplinePointsType

class NXOpen.Features.PointSetBuilderSplinePointsType

Bases: object

The settings for the spline points definition.

Enum Members

Enum Member Enum Member Description
DefiningPoints
Points will be created at spline defining points.
Knots
Points will be created at spline knot points.
Poles
Points will be created at spline pole points.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.