PointSetBuilderPatternLimitsType Enumeration¶
NXOpen.Features.PointSetBuilder.PatternLimitsType is an alias for NXOpen.Features.PointSetBuilderPatternLimitsType
-
class
NXOpen.Features.
PointSetBuilderPatternLimitsType
¶ Bases:
object
The settings for the pattern limit definition.
Enum Members
Enum Member Enum Member Description DiagonalPoints The pattern limit is defined by two points.Percentages The pattern limit is defined by surface U and V values.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-