PointSetBuilderFacePointsType Enumeration¶
NXOpen.Features.PointSetBuilder.FacePointsType is an alias for NXOpen.Features.PointSetBuilderFacePointsType
-
class
NXOpen.Features.
PointSetBuilderFacePointsType
¶ Bases:
object
The settings for the face points definition.
Enum Members
Enum Member Enum Member Description Pattern Points will be created based on a defined pattern.FacePercentage A point will be created at given face percentages.BSurfacePoles Points will be created at surface poles.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-