PatternFeatureBuilderPatternMethodOptions Enumeration

NXOpen.Features.PatternFeatureBuilder.PatternMethodOptions is an alias for NXOpen.Features.PatternFeatureBuilderPatternMethodOptions

class NXOpen.Features.PatternFeatureBuilderPatternMethodOptions

Bases: object

the Pattern method options.

Enum Members

Enum Member Enum Member Description
Variational
variational
Simple
simple
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.