PatternFeatureBuilderOutputOptions Enumeration

NXOpen.Features.PatternFeatureBuilder.OutputOptions is an alias for NXOpen.Features.PatternFeatureBuilderOutputOptions

class NXOpen.Features.PatternFeatureBuilderOutputOptions

Bases: object

the Output options.

Enum Members

Enum Member Enum Member Description
PatternFeature
Pattern Feature
CopiesOfInputFeatures
Copies of Input features
CopiesOfInputFeaturesInGroup
Copies of Input features in Group
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.