PatternFaceBuilderPatternTypes Enumeration

NXOpen.Features.PatternFaceBuilder.PatternTypes is an alias for NXOpen.Features.PatternFaceBuilderPatternTypes

class NXOpen.Features.PatternFaceBuilderPatternTypes

Bases: object

Enumeration of pattern type, don’t use it until nx502

New in version NX5.0.2.

Enum Members

Enum Member Enum Member Description
Rectangular
This stands for rectangular pattern type.
Circular
This stands for circular pattern type.
Mirror
This stands for mirror pattern type.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.