PatchOpeningsBuilderTypes Enumeration

NXOpen.Features.PatchOpeningsBuilder.Types is an alias for NXOpen.Features.PatchOpeningsBuilderTypes

class NXOpen.Features.PatchOpeningsBuilderTypes

Bases: object

The method used to patch the opening

Enum Members

Enum Member Enum Member Description
Quilted
Patch with quilted patchwork of faces
NSided
Patch with N-sided surface area method
Mesh
Patch with through curve mesh
ByDeletingEdges
Patch by deleting edges and growing faces
Extension
Tangent edge extension method
Notch
Notch fill method
Joggle
Joggle fill method
MoldWizard
Patch with Mold wizard edge patch method
BySuppression
Patch by suppressing features
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.