PartModuleBuilder Class¶
-
class
NXOpen.Features.
PartModuleBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.PartModule
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreatePartModuleBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ActivatePartModule | Returns or sets the option indicating whether part module is to be activated. |
InputReferences | Returns the part module input references. |
Name | Returns or sets the part module name |
Name1 | Returns or sets the part module name |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ShowOnlyPartModule | Returns or sets the option indicating whether only part module contents are to be shown. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ActivatePartModule¶
-
PartModuleBuilder.
ActivatePartModule
¶ Returns or sets the option indicating whether part module is to be activated.
If true, the part module will be activated, else, part module will be deactivated
-------------------------------------
Getter Method
Signature
ActivatePartModule()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActivatePartModule(activate)
Parameters: activate (bool) – New in version NX8.0.0.
License requirements: usr_defined_features (“USER DEFINED FEATURES”)
InputReferences¶
-
PartModuleBuilder.
InputReferences
¶ Returns the part module input references.
This API is now deprecated. Please use
GeometricUtilities.PartModuleInputBuilder.InputReferences()
instead.-------------------------------------
Getter Method
Signature
InputReferences()
Returns: Return type: NXOpen.GeometricUtilities.PartModuleReferencesBuilder
New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
GeometricUtilities.PartModuleInputBuilder.InputReferences()
instead.License requirements: None.
Name¶
-
PartModuleBuilder.
Name
¶ Returns or sets the part module name
This API is now deprecated. Please use
Features.PartModuleBuilder.Name1()
instead.-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
Features.PartModuleBuilder.Name1()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
Features.PartModuleBuilder.Name1()
instead.License requirements: usr_defined_features (“USER DEFINED FEATURES”)
Name1¶
-
PartModuleBuilder.
Name1
¶ Returns or sets the part module name
-------------------------------------
Getter Method
Signature
Name1()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name1(name)
Parameters: name (str) – New in version NX9.0.0.
License requirements: usr_defined_features (“USER DEFINED FEATURES”)
ShowOnlyPartModule¶
-
PartModuleBuilder.
ShowOnlyPartModule
¶ Returns or sets the option indicating whether only part module contents are to be shown.
If true, only displayable objects in the part module will be shown. Else, no action is taken.
This API is now deprecated. Please use
NXOpen.Features.PartModule.ShowOnly()
instead.-------------------------------------
Getter Method
Signature
ShowOnlyPartModule()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.Features.PartModule.ShowOnly()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ShowOnlyPartModule(showOnly)
Parameters: showOnly (bool) – New in version NX8.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.Features.PartModule.ShowOnly()
instead.License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
PartModuleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.