PartGeometryCopyBuilderType Enumeration¶
NXOpen.Features.PartGeometryCopyBuilder.Type is an alias for NXOpen.Features.PartGeometryCopyBuilderType
-
class
NXOpen.Features.
PartGeometryCopyBuilderType
¶ Bases:
object
Specifies object types to copy in the part geometry copy block
Enum Members
Enum Member Enum Member Description Automatic An option to select point, datum, sketch, body, and curve featureBodyCollector An option to select bodies via body selection intentBodyObject An option to select body, body-based feature, and body groupCurveFeature Curve-based featureSketch Sketch featureDatum Datum plane, datum axis or datum coordinate system featurePoint PointCompositeCurve An option to composite a curve via curve selection intentCompositeFace An option to composite a body via face selection intentExpression ExpressionPmi PMI dimensionCurve Curve or edgeFace FaceRoutingObject Routing Object-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-