OutputFeatureData Class¶
-
class
NXOpen.Features.
OutputFeatureData
¶ Bases:
NXOpen.TransientObject
JA interface for the OutputFeatureData object
An instance of this class can be obtained from
NXOpen.Features.CustomFeaturePostUpdateEvent.CreateOutputFeatureData()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ShowInGraphicView | Returns or sets the output feature visibility in Graphic View |
Methods¶
Method | Description |
---|---|
Dispose | Frees the memory associated with this object. |
GetFeature | Get the feature @return The Output Feature |
Property Detail¶
ShowInGraphicView¶
-
OutputFeatureData.
ShowInGraphicView
¶ Returns or sets the output feature visibility in Graphic View
-------------------------------------
Getter Method
Signature
ShowInGraphicView()
Returns: True if the feature to be visible in Graphic View else false Return type: bool New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
-------------------------------------
Setter Method
Signature
ShowInGraphicView(showInGraphicView)
Parameters: showInGraphicView (bool) – True if the feature to be visible in Graphic View else false New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Dispose¶
-
OutputFeatureData.
Dispose
¶ Frees the memory associated with this object.
After invocation of this method, the object is no longer valid.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetFeature¶
-
OutputFeatureData.
GetFeature
¶ Get the feature
Signature
GetFeature()
Returns: The Output Feature Return type: NXOpen.Features.Feature
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)