OffsetSurfaceBuilderOutputOptionType Enumeration¶
NXOpen.Features.OffsetSurfaceBuilder.OutputOptionType is an alias for NXOpen.Features.OffsetSurfaceBuilderOutputOptionType
-
class
NXOpen.Features.
OffsetSurfaceBuilderOutputOptionType
¶ Bases:
object
Represents the type of output option.
The faces to be offset can be disconnected and also from multiple bodies. If either is the case, then multiple features are created. For deciding whether there should be one feature for each topologically connected set of faces or one feature for each face selected the enum below has been provided
Enum Members
Enum Member Enum Member Description OneFeatureForConnectedFaces OneFeatureForEachFace OneFeatureForAllFaces -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-