OffsetEmbossBuilderTypes Enumeration

NXOpen.Features.OffsetEmbossBuilder.Types is an alias for NXOpen.Features.OffsetEmbossBuilderTypes

class NXOpen.Features.OffsetEmbossBuilderTypes

Bases: object

Enumeration of center types

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
Curve
This stands for curve case.
Point
This stands for point case.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.