OffsetCurveBuilderTypes Enumeration

NXOpen.Features.OffsetCurveBuilder.Types is an alias for NXOpen.Features.OffsetCurveBuilderTypes

class NXOpen.Features.OffsetCurveBuilderTypes

Bases: object

Represents the Offset Curve types

Enum Members

Enum Member Enum Member Description
Distance
Distance
Draft
Draft
LawControl
Law Control
Axial3d
3D Axial
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.