MirrorFaceBuilderMirrorPlaneOptions Enumeration

NXOpen.Features.MirrorFaceBuilder.MirrorPlaneOptions is an alias for NXOpen.Features.MirrorFaceBuilderMirrorPlaneOptions

class NXOpen.Features.MirrorFaceBuilderMirrorPlaneOptions

Bases: object

Represents the mirror plane options

Enum Members

Enum Member Enum Member Description
Existing
Existing Plane
New
New Plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.