MirrorCurveBuilderPlaneOptions Enumeration

NXOpen.Features.MirrorCurveBuilder.PlaneOptions is an alias for NXOpen.Features.MirrorCurveBuilderPlaneOptions

class NXOpen.Features.MirrorCurveBuilderPlaneOptions

Bases: object

Represents the Plane options.

Enum Members

Enum Member Enum Member Description
ExistingPlane
existing plane
NewPlane
new plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.