MirrorBodyBuilderFeatureOptionType Enumeration¶
NXOpen.Features.MirrorBodyBuilder.FeatureOptionType is an alias for NXOpen.Features.MirrorBodyBuilderFeatureOptionType
-
class
NXOpen.Features.
MirrorBodyBuilderFeatureOptionType
¶ Bases:
object
enum for feature option type
Enum Members
Enum Member Enum Member Description OneFeatureForAllBodies An option to create one mirror or linked mirror body feature for all selected bodies as body collectorSeparateFeatureForEachBody An option to create a separate mirror or linked mirror body feature per single body-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-