MidSurfaceUserDefinedBuilder Class¶
-
class
NXOpen.Features.
MidSurfaceUserDefinedBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.MidSurfaceUserDefined
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateMidSurfaceUserDefinedBuilder()
Default values.
Property Value MaxThickness.Value 0 (millimeters part), 0 (inches part) MinThickness.Value 0 (millimeters part), 0 (inches part) OutsideThickness.Value 0 (millimeters part), 0 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
MaxThickness | Returns the max thickness allowed during Fem solve |
MinThickness | Returns the min element thickness allowed during Fem solve |
OutsideThickness | Returns the outside thickness to be used during Fem solve if the node falls outside of solid |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SheetBodySelection | Returns the sheet bodies to be treated as user defined neutral sheets |
SolidBodySel | Returns the solid body for user defined midsurface |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MaxThickness¶
-
MidSurfaceUserDefinedBuilder.
MaxThickness
¶ Returns the max thickness allowed during Fem solve
-------------------------------------
Getter Method
Signature
MaxThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MinThickness¶
-
MidSurfaceUserDefinedBuilder.
MinThickness
¶ Returns the min element thickness allowed during Fem solve
-------------------------------------
Getter Method
Signature
MinThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
OutsideThickness¶
-
MidSurfaceUserDefinedBuilder.
OutsideThickness
¶ Returns the outside thickness to be used during Fem solve if the node falls outside of solid
-------------------------------------
Getter Method
Signature
OutsideThickness()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
SheetBodySelection¶
-
MidSurfaceUserDefinedBuilder.
SheetBodySelection
¶ Returns the sheet bodies to be treated as user defined neutral sheets
-------------------------------------
Getter Method
Signature
SheetBodySelection()
Returns: Return type: NXOpen.SelectBodyList
New in version NX7.5.0.
License requirements: None.
SolidBodySel¶
-
MidSurfaceUserDefinedBuilder.
SolidBodySel
¶ Returns the solid body for user defined midsurface
-------------------------------------
Getter Method
Signature
SolidBodySel()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
MidSurfaceUserDefinedBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.