MeshTransformerBuilderSmoothingType Enumeration

NXOpen.Features.MeshTransformerBuilder.SmoothingType is an alias for NXOpen.Features.MeshTransformerBuilderSmoothingType

class NXOpen.Features.MeshTransformerBuilderSmoothingType

Bases: object

Smoothing option type

Enum Members

Enum Member Enum Member Description
VeryLow
Smoothing very low
Low
Smoothing low
Normal
Smoothing normal
High
Smoothing high
VeryHigh
Smoothing high
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.