MeshTransformerBuilderMeshTopologyType Enumeration

NXOpen.Features.MeshTransformerBuilder.MeshTopologyType is an alias for NXOpen.Features.MeshTransformerBuilderMeshTopologyType

class NXOpen.Features.MeshTransformerBuilderMeshTopologyType

Bases: object

Mesh topology option type

Enum Members

Enum Member Enum Member Description
Aligned
Aligned
Unaligned
Unaligned
EndOnly
End only
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.