MeshTransformerBuilderContinuityType Enumeration

NXOpen.Features.MeshTransformerBuilder.ContinuityType is an alias for NXOpen.Features.MeshTransformerBuilderContinuityType

class NXOpen.Features.MeshTransformerBuilderContinuityType

Bases: object

Continuity type

Enum Members

Enum Member Enum Member Description
C2
C2 continuity
C4
C4 continuity
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.