MatchEdgeBuilderTypes Enumeration¶
NXOpen.Features.MatchEdgeBuilder.Types is an alias for NXOpen.Features.MatchEdgeBuilderTypes
-
class
NXOpen.Features.
MatchEdgeBuilderTypes
¶ Bases:
object
Match Edge match types.
The match to datum type is deprecated in NX7.0.
Enum Members
This type deprecated in NX7.0. Use
NXOpen.Features.EdgeSymmetry
feature instead. “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-