MatchEdgeBuilderPoleMovementConstraintEnumType Enumeration

NXOpen.Features.MatchEdgeBuilder.PoleMovementConstraintEnumType is an alias for NXOpen.Features.MatchEdgeBuilderPoleMovementConstraintEnumType

class NXOpen.Features.MatchEdgeBuilderPoleMovementConstraintEnumType

Bases: object

Pole movement type

Enum Members

Enum Member Enum Member Description
WCS
Along WCS X/Y/Z direction
View
Along view
Vector
Along user defined vector
Normal
Normal
Project
Project
Inherit
Inherit
FixStart
Fix start
FixEnd
Fix end
StartAndEnd
Fix start and end
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.