LinearDimensionBuilderOrientationOptionType Enumeration

NXOpen.Features.LinearDimensionBuilder.OrientationOptionType is an alias for NXOpen.Features.LinearDimensionBuilderOrientationOptionType

class NXOpen.Features.LinearDimensionBuilderOrientationOptionType

Bases: object

the option that controls whether the OrientXpress or whether the vector block Controls the orientation of the Linear Dimension

Enum Members

Enum Member Enum Member Description
OrientXpress
Orientation option using Orient Xpress
Vector
Orientation option using vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.