LawExtensionBuilderExTypes Enumeration

NXOpen.Features.LawExtensionBuilderEx.Types is an alias for NXOpen.Features.LawExtensionBuilderExTypes

class NXOpen.Features.LawExtensionBuilderExTypes

Bases: object

Law extension creation types

Enum Members

Enum Member Enum Member Description
Faces
Reference faces
Vector
Reference vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.