IsoparametricCurvesBuilderPlacementTypes Enumeration

NXOpen.Features.IsoparametricCurvesBuilder.PlacementTypes is an alias for NXOpen.Features.IsoparametricCurvesBuilderPlacementTypes

class NXOpen.Features.IsoparametricCurvesBuilderPlacementTypes

Bases: object

Curve creation options

Enum Members

Enum Member Enum Member Description
Uniform
Insert curves uniformly
ThroughPoints
Insert curves through points
BetweenPoints
Insert curves between points
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.