IsoparametricCurvesBuilderDirectionTypes Enumeration

NXOpen.Features.IsoparametricCurvesBuilder.DirectionTypes is an alias for NXOpen.Features.IsoparametricCurvesBuilderDirectionTypes

class NXOpen.Features.IsoparametricCurvesBuilderDirectionTypes

Bases: object

Curve direction options

Enum Members

Enum Member Enum Member Description
IsoU
Iso U direction
IsoV
Iso V direction
IsoUV
Iso U and Iso V direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.