IsoclineCurveBuilder Class¶
-
class
NXOpen.Features.
IsoclineCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
Features.IsoclineCurve
builderTo create a new instance of this class, use
NXOpen.Features.FreeformCurveCollection.CreateIsoclineCurveBuilder()
Default values.
Property Value CurveFitData.CurveJoinMethod No CurveFitData.Degree 7 CurveFitData.FitMethod DegreeAndSegments CurveFitData.IsAdvancedFit 0 CurveFitData.IsAlignShape 0 CurveFitData.MaximumDegree 7 CurveFitData.MaximumSegments 1 CurveFitData.MinimumDegree 5 CurveFitData.Segments 1 DistanceThreshold 0.25 (millimeters part), 0.01 (inches part) EndAngle.Value 90 IntervalAngle.Value 10 StartAngle.Value -90 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CanOptimizeCurve | Returns or sets the Optimize Curve |
CurveFitData | Returns the curve fitting parameters |
DistanceThreshold | Returns or sets the distance threshold |
EndAngle | Returns the end angle |
Face | Returns the select face |
IntervalAngle | Returns the interval angle |
IsAssociative | Returns or sets the associative |
IsoclineAngle | Returns the isocline angle |
IsoclineTypes | Returns or sets the isocline types |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReferenceDirection | Returns or sets the reference direction |
StartAngle | Returns the start angle |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateIsocline | Creates isocline curves |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IsoclineCurveBuilderCurveTypes Enumeration | The option indicating number of curves to be created |
Property Detail¶
CanOptimizeCurve¶
-
IsoclineCurveBuilder.
CanOptimizeCurve
¶ Returns or sets the Optimize Curve
-------------------------------------
Getter Method
Signature
CanOptimizeCurve()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanOptimizeCurve(canOptimizeCurve)
Parameters: canOptimizeCurve (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
CurveFitData¶
-
IsoclineCurveBuilder.
CurveFitData
¶ Returns the curve fitting parameters
-------------------------------------
Getter Method
Signature
CurveFitData()
Returns: Return type: NXOpen.GeometricUtilities.CurveFitData
New in version NX11.0.0.
License requirements: None.
DistanceThreshold¶
-
IsoclineCurveBuilder.
DistanceThreshold
¶ Returns or sets the distance threshold
-------------------------------------
Getter Method
Signature
DistanceThreshold()
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceThreshold(distanceThreshold)
Parameters: distanceThreshold (float) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
EndAngle¶
-
IsoclineCurveBuilder.
EndAngle
¶ Returns the end angle
-------------------------------------
Getter Method
Signature
EndAngle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Face¶
-
IsoclineCurveBuilder.
Face
¶ Returns the select face
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.ScCollector
New in version NX11.0.0.
License requirements: None.
IntervalAngle¶
-
IsoclineCurveBuilder.
IntervalAngle
¶ Returns the interval angle
-------------------------------------
Getter Method
Signature
IntervalAngle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
IsAssociative¶
-
IsoclineCurveBuilder.
IsAssociative
¶ Returns or sets the associative
-------------------------------------
Getter Method
Signature
IsAssociative()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAssociative(isAssociative)
Parameters: isAssociative (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsoclineAngle¶
-
IsoclineCurveBuilder.
IsoclineAngle
¶ Returns the isocline angle
-------------------------------------
Getter Method
Signature
IsoclineAngle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
IsoclineTypes¶
-
IsoclineCurveBuilder.
IsoclineTypes
¶ Returns or sets the isocline types
-------------------------------------
Getter Method
Signature
IsoclineTypes()
Returns: Return type: NXOpen.Features.IsoclineCurveBuilderCurveTypes
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsoclineTypes(isoclineTypes)
Parameters: isoclineTypes ( NXOpen.Features.IsoclineCurveBuilderCurveTypes
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ReferenceDirection¶
-
IsoclineCurveBuilder.
ReferenceDirection
¶ Returns or sets the reference direction
-------------------------------------
Getter Method
Signature
ReferenceDirection()
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceDirection(referenceDirection)
Parameters: referenceDirection ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
StartAngle¶
-
IsoclineCurveBuilder.
StartAngle
¶ Returns the start angle
-------------------------------------
Getter Method
Signature
StartAngle()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
CreateIsocline¶
-
IsoclineCurveBuilder.
CreateIsocline
¶ Creates isocline curves
Signature
CreateIsocline()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
IsoclineCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.