IFormBuilderTransitionTypes Enumeration

NXOpen.Features.IFormBuilder.TransitionTypes is an alias for NXOpen.Features.IFormBuilderTransitionTypes

class NXOpen.Features.IFormBuilderTransitionTypes

Bases: object

Transition options of the surface

Enum Members

Enum Member Enum Member Description
Local
Local transition
Global
Global transition
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.