HoleSubtype Enumeration

NXOpen.Features.Hole.Subtype is an alias for NXOpen.Features.HoleSubtype

class NXOpen.Features.HoleSubtype

Bases: object

Represents the subtype of the hole

Enum Members

Enum Member Enum Member Description
Simple
Simple hole
Counterbore
Counterbore hole
Countersink
Countersink hole
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.