HolePackageBuilderHoleDepthLimitOptions Enumeration

NXOpen.Features.HolePackageBuilder.HoleDepthLimitOptions is an alias for NXOpen.Features.HolePackageBuilderHoleDepthLimitOptions

class NXOpen.Features.HolePackageBuilderHoleDepthLimitOptions

Bases: object

Represents hole depth limit options.

Enum Members

Enum Member Enum Member Description
Value
Value limit options
UntilSelected
Until selected limit options
UntilNext
Until next limit options
ThroughBody
Through body limit options
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.