GuidedExtensionBuilderExTypes Enumeration

NXOpen.Features.GuidedExtensionBuilderEx.Types is an alias for NXOpen.Features.GuidedExtensionBuilderExTypes

class NXOpen.Features.GuidedExtensionBuilderExTypes

Bases: object

Option types to create guided extension surface

Enum Members

Enum Member Enum Member Description
TangentFromFaces
Extend tangentially from faces
Vector
Perpendicular to a vector
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.