GlobalShapingBuilderTransitionType Enumeration

NXOpen.Features.GlobalShapingBuilder.TransitionType is an alias for NXOpen.Features.GlobalShapingBuilderTransitionType

class NXOpen.Features.GlobalShapingBuilderTransitionType

Bases: object

Represents the transition method type.

Enum Members

Enum Member Enum Member Description
Function1
Tangent continuous transition
Function2
Position continuous transition
Law
Transition by law
G2
g2 continuous
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.