GlobalShapingBuilderRotationMethod Enumeration

NXOpen.Features.GlobalShapingBuilder.RotationMethod is an alias for NXOpen.Features.GlobalShapingBuilderRotationMethod

class NXOpen.Features.GlobalShapingBuilderRotationMethod

Bases: object

Represents the rotation method type.

Enum Members

Enum Member Enum Member Description
Constant
Constant anlge rotation
LawControlled
Law controlled rotation
CurveDefined
Curve interpolated rotation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.