GlobalShapingBuilderOffsetMethod Enumeration

NXOpen.Features.GlobalShapingBuilder.OffsetMethod is an alias for NXOpen.Features.GlobalShapingBuilderOffsetMethod

class NXOpen.Features.GlobalShapingBuilderOffsetMethod

Bases: object

Represents the offset method type.

Enum Members

Enum Member Enum Member Description
Constant
Constant offset
LawControlled
Law controlled
CurveDefined
Curve interpolated
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.