GlobalShapingBuilderModifyMethodType Enumeration

NXOpen.Features.GlobalShapingBuilder.ModifyMethodType is an alias for NXOpen.Features.GlobalShapingBuilderModifyMethodType

class NXOpen.Features.GlobalShapingBuilderModifyMethodType

Bases: object

Represent surface modify method.

Enum Members

Enum Member Enum Member Description
Stretch
By Surface stretch modify
Overcrown
By Surface overcrown modify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.