GlobalShapingBuilderDeformationTypeValues Enumeration¶
NXOpen.Features.GlobalShapingBuilder.DeformationTypeValues is an alias for NXOpen.Features.GlobalShapingBuilderDeformationTypeValues
-
class
NXOpen.Features.
GlobalShapingBuilderDeformationTypeValues
¶ Bases:
object
Represents the deformation type.
Enum Members
Enum Member Enum Member Description ToPoint To pointToCurves To curvesOpenRegion Open regionWallDeformation Wall deformationOverbend OverbendMatchToSheet Match to sheetStretchToPoint Stretch to pointStretchToCurve Stretch to curveRadiusReduction Radius ReductionBySurface - Old By surface method
ByCurve (10)Bend/Twist by curvesUnknown Unknown deformation-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.