GlobalShapingBuilderDeformBodyType Enumeration

NXOpen.Features.GlobalShapingBuilder.DeformBodyType is an alias for NXOpen.Features.GlobalShapingBuilderDeformBodyType

class NXOpen.Features.GlobalShapingBuilderDeformBodyType

Bases: object

Represent sheet deformation type.

Enum Members

Enum Member Enum Member Description
SheetBodies
Sheet bodies
FacetBodies
Facet bodies
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.