GlobalShapingBuilderBodyMethod Enumeration

NXOpen.Features.GlobalShapingBuilder.BodyMethod is an alias for NXOpen.Features.GlobalShapingBuilderBodyMethod

class NXOpen.Features.GlobalShapingBuilderBodyMethod

Bases: object

Represents the body method type.

Enum Members

Enum Member Enum Member Description
Solid
Output solid
Sheet
Output sheet
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.