GeometricConstraintDataParameterDirection Enumeration

NXOpen.Features.GeometricConstraintData.ParameterDirection is an alias for NXOpen.Features.GeometricConstraintDataParameterDirection

class NXOpen.Features.GeometricConstraintDataParameterDirection

Bases: object

Parameter direction to be used for creation of the constraint at a point which is attached to an object, for example a curve or a face

Enum Members

Enum Member Enum Member Description
Iso
Iso parameter
Section
General section if point is attached to face
Normal
Normal
Perpendicular
Perpendicular to curve on face or edge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.